Proven technology at work in some of the world's toughest environments
"Space is at a premium offshore, and you only have a certain footprint you can work with. Danfoss pumps are ideal for this. They don't weigh much and their design is simple and easy to work with. Whereas membrane pumps have to be adjusted inside the pump house, Danfoss CLP pumps don't require much adjustment and can be adjusted externally."
"Engineers in purchasing have technical responsibility for a huge number of components," says Thomas Broge. "In many cases, the main selection criteria is price, but if we notice that something keeps breaking down and needs to be repaired, we start to dig in and investigate what is going wrong. Danfoss CLP pumps have worked well in Tyra. They have a long lifetime and long service intervals. We have been quite satisfied with the pumps, their low maintenance needs and the fact that Danfoss is always willing to provide good service."
"Reliability is a given, but we were especially looking for high-capacity pumps that don't take up much room. The Danfoss CLP pumps deliver on both counts"
"We are often pioneers in new technology, so the idea of trying something new is not foreign to us."
"We thought we had a problem with one of the pumps shortly after installation. We called Danfoss to let them know, and less than 24 hours later a brand new pump had been flown out to the rig. That is service. It turns out that there was actually nothing wrong with the pump, but that is beside the point. We depend on 100% uptime, and having onfidence in our suppliers is a must. Danfoss has delivered on all counts."